Hi, I want to use the AD4115 with switched power-supplies. Do they have negative impact on accuracy?
The application is a Battery Management System (BMS), sampling every second voltage, amperes and temperatures. During main of that second, the current used b the BMS should be at low as possible. A switched power-supply (i.e. MAX25232 or LM33630, or a AD alternative not searched for yet) can operate in High Efficiency with low load.
The most accuracy needed is measurings amps during charge or load, from some mA up to 200A.