AD7770
Recommended for New Designs
The AD7770 is an 8-channel, simultaneous sampling ADC. Eight
full sigma-delta (Σ-Δ) ADCs are on chip. The AD7770 provides
a low input current to allow...
Datasheet
AD7770 on Analog.com
Hi
AD7770 ADC data can be read by the following table given in datasheet
Please let us know how can we calculate the ADC digital output code for the different voltage levels(2.1168V, 2.16V, 2.2032V)
As per our design we are external Vref of 3.3V
Please provide the digital output code for the full scale range of 3.3V
Thanks and Regards
Abishek V
Hi Abishek
The following function is the one I am currently using and it seems to work properly.
ref= value of the reference
raw_code= the 24bits data
voltage= pointer where the calculated voltage is stored.
void ad7771_data_to_voltage(double ref, uint32_t *raw_code, double *voltage)
{
if((*raw_code <= 0x7FFFFF) && (*raw_code >= 0x00))
{
*voltage = (double)(*raw_code * (ref/16777216.0));
}
else
{
*voltage = (double)((*raw_code * (ref/16777216.0))-ref);
}
}
This excel file will help you calculate the voltage. You only need to insert in the blue cell the value read from the ADC.
Regards
Joan
This excel file will help you calculate the voltage. You only need to insert in the blue cell the value read from the ADC.
Regards
Joan