Post Go back to editing

About ERR_DAT of GPIO CONFIGURATION REGISTER (0x06) of AD4111

Hello

I have a question about GPIO CONFIGURATION REGISTER (0x06) for AD4111.

In the explanation of ERR_DAT on P52, there is a description about the input and the operation as a GPO, but there is no description in the open drain error mode.


If the bit is set to 10 in the explanation of ERR_EN, the result of the OR operation of the status register is inverted and reflected in the Error pin.

Is it okay to recognize that ERR_DAT reads back the status of the Error pin when ERR_EN is set to 10?

I would be grateful if you could reply.

Best Regards,
Knj

Parents Reply Children
No Data