Hi all,
Is it okay to always input the clock to LTC2324-14?
Best Regards,
Leo
LTC2324-14
Production
The LTC2324-14 is a low noise, high speed quad 14-bit + sign successive approximation register (SAR) ADC with differential inputs and wide input common...
Datasheet
LTC2324-14 on Analog.com
Hi all,
Is it okay to always input the clock to LTC2324-14?
Best Regards,
Leo
Hi,
Why do you mean by always? Does it means even when the device is powered down?
As a good practice we do not recommend to apply any analog or digital inputs when supplies are power off. May I know the reason for the asked? Is it not possible to disable the clock when the device is powered down?
However, I don't think it will potentially damage the part if the current input is very small. Do you know the current input at the clock pins? And what do you mean by power off like supply pins are floating or connected to GND?
Thanks,
Jellenie
On another thought. Does it means continuously supplying the SCLK even if you are not going to communicate (write or read)? I don't think that is also a good a practice. Excessive or incorrect number of SCLKs may affect synchronization of the interface. It may also be a cause of miscommunication.
Thanks,
Jellenie
Sorry for the lack of explanation. it is possible to disable the clock when LTC2324-14 is power down.
Yes, I think you understand the point of my question.
It seems like it is not good to supply continuously SCLK even if not going to communicate(yes, LTC2324-14 also needs to be powered on in this case). I will use an FPGA to access LTC2324-14 and consider how to make and supply SCLK to LTC2324-14
So, as your recommendation, Supplying SCLK referring to CNV Signal is good, and do not supply a continuous SCLK, am I right?
Best Regards,
Hi,
Yes, providing the required or correct number of SCLK cycles only is recommended to avoid any issues.
I think you can refer to the timing diagram in the datasheet. So when communication with the interface is completed the SCK is idle (low).
Thanks,
Jellenie
Hi,
I'm sorry I'm confused with this follow up question? The SCK is controlled by the external processor so I guess it should be possible. Or can you clarify the question here please?
Thanks,
Jellenie
Hi,
Thank you for the quick support!
Best Regards,