AD7761
Production
The AD7761 is an 8-channel, simultaneous sampling sigma-delta (Σ-Δ) analog-to-digital converter (ADC) with a Σ-Δ modulator and digital filter per channel...
Datasheet
AD7761 on Analog.com
AD7768
Recommended for New Designs
The AD7768/AD7768-4 are 8-channel and 4-channel 24-bit, simultaneous sampling, sigma-delta (Σ-Δ) analog-to-digital converters (ADCs) with power scaling...
Datasheet
AD7768 on Analog.com
AD7768-1
Recommended for New Designs
The AD7768-1 is a low power, high performance, Σ-Δ analog-to-digital converter (ADC), with a Σ-Δ modulator and digital
filter for precision conversion...
Datasheet
AD7768-1 on Analog.com
AD7768-4
Recommended for New Designs
The AD7768/AD7768-4 are 8-channel and 4-channel 24-bit, simultaneous sampling, sigma-delta (Σ-Δ) analog-to-digital converters (ADCs) with power scaling...
Datasheet
AD7768-4 on Analog.com
Hi,
I need to use the web tool "Precision ADC Driver Tool" to calculate the RC filter for the driver but there is no AD7761. The only one close is AD7768, AD7768-1 and AD7768-4.
Is it ok if I use any of these?
Thanks!
Hi,
AD7761 is a 16 bit version of AD7768 which is a 24 bit ADC. These parts are from the same family and the majority of behavior is the same. However, you have to consider that they are different in terms of resolution. So whatever noise contributions you get from the system I guess if it is lower than the LSB size of AD7761 then SNR, Dynamic range, etc. would still be limited by the LSB size. So I am not sure if it make sense to use AD7768 from the tool in order to simulate the expected performance of AD7761. But my thinking is that whatever the tool calculates for external RC values should work with AD7761 but like I said the performance would still be limited by the actual resolution.
I will also ask the product apps for these parts and see what his thoughts on this.
Thanks,
Jellenie
Hi Nick
i dont think we can use it, please let mw know your settings to advise on the RC filter
thanks