AD7327: Control setting and Conversion Data read for "Fully Differential Input Mode" and "Pseudo Differential Input Mode"

Hi,

Couple of queries on AD3727

1. For setting 8 inputs as "4 Fully Differential Inputs" (Mode 1 = 1, Mode 0 = 0) or "4 Pseudo Differential Inputs" (Mode 1 = 0, Mode 0 = 1) whether user has to write 8 times Control Word with appropriate ADD2, ADD1 and ADD0 and corresponding mode bits or 4 times with ADD2:1 = 0, 3,4,7? Why i asked this question is that, if Mode is selected as AD, the analog inputs are fixed for ADD (0 and 1 ) or (2 and 3) or (4 and 5) or (6 and 7). 

2. Similarly what the Channel Identification number in DOUT while inputs configured Fully Diff or Pseudo Diff? 

with regards

Rajeeva GK