AD7606C-18

So, im using the ad7606c-18 instead of the -16, and I use a SCLK with 16.67 MHz and works correctly, but when I increase it to 25 MHz it does not work. I'm using the EVAL-AD7606C18FMCZ board.

Another question that I have, if you know if the FlexSPI from NXP LS1028 can be adapted to this serial protocol?, I think we cannot, just to confirm.

And what SPI protocol has more than one MISO signal?

Thanks.

Parents
  • By the way, if I write and read a adc register at 16MHz works ok, so I do read/write into registers at that speed.

    If I read the converted values (adc mode) at 25 MHz at it seems to have the correct value, I have a problem there in my microcontroller but in the analyzer I have the correct value, but if I read the converted values at 50MHz it does not work, I see another value.

Reply
  • By the way, if I write and read a adc register at 16MHz works ok, so I do read/write into registers at that speed.

    If I read the converted values (adc mode) at 25 MHz at it seems to have the correct value, I have a problem there in my microcontroller but in the analyzer I have the correct value, but if I read the converted values at 50MHz it does not work, I see another value.

Children