Post Go back to editing

AD7746 liquid level monitoring

Thread Summary

The user is experiencing unstable capacitance readings and hitting the maximum level (4pF) when using a custom ruler with the EVAL-AD7746EBZ for liquid level monitoring. The final answer suggests using the equation in Figure 5 for ruler design and extending the capacitance range with techniques from AN-1585. Additional advice includes applying grounding and shielding around the sensor pads, using the same EXCA+EXCB for both CIN1 and CIN2, and performing offset and gain calibration to accurately measure capacitance with CAPDAC enabled.
AI Generated Content

Hello guy,

My application is similar to liquid level monitoring method that described below, pasting the ruler outside the container and monitor the liquid level inside the container.

https://www.analog.com/en/analog-dialogue/articles/capacitance-to-digital-converter-technology-healthcare.html

We build our own the ruler (~5cm x ~2cm and without grounding) and connect 4 wires to EVAL-AD7746EBZ and then showing the capacity and water level on PC software "AD7746 Capacitive Level Sensor Demo v2.2", the result is what we expected but when we build a longer ruler, the capacity value is very unstable and easy to hit the maximum level 4pF when inside have water.

Below are my questions:

1)  We keep searching on Engineer Zone, but cannot find any reference circuit about EVAL-AD7746LDZ and any design guideline for the "Ruler" that may fit for our application?

2) Is it possible to calculate / design the PCB traces for measuring over 30 cm of water if just pasting outside the container?

3) Is there any way to adjust the maximum capacity level if keep using the PC software?

 

Thank and regards,

Kevin

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.