Dear Sir,
We have the question about LTC2360 SPI I/F.
We understand that LTC2360 output SDO when COV(CS) is High to Low .
We would like to get the continuous SDO data when keeping LOW.
Image is as follows picture. Can it support this function?

KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC2360
Production
The LTC2360/LTC2361/LTC2362 are 100ksps/250ksps/500ksps, 12-bit, sampling A/D converters that draw only 0.5mA, 0.75mA and 1.1mA, respectively, from a single...
Datasheet
LTC2360 on Analog.com
Dear Sir,
We have the question about LTC2360 SPI I/F.
We understand that LTC2360 output SDO when COV(CS) is High to Low .
We would like to get the continuous SDO data when keeping LOW.
Image is as follows picture. Can it support this function?

Hi,
This is not possible. The LTC2360 only produces new data when CONV is taken high and then brought low. If you only have two lines available, I would suggest using the LTC2301 which uses the I2C interface.
Dear Ghoover-san,
Thank you for you reply,noted. We check LTC2301 specification.