Post Go back to editing

LTC2380-24 Multiplexing

Thread Summary

The user wants to multiplex the LTC2380 for 2 channels and handle a bipolar signal from a preamplifier. The support engineer suggests using a fully differential amplifier like the ADA4945-1 to translate the bipolar signal and drive the cable, noting the MAX4618 MUX has higher distortion. The LTC2380-24 offers better THD and SNR, while the AD7641 has an internal reference. For multiplexing, the user should allow for signal settling time after channel changes.
AI Generated Content

Good evening!

I'd like to multiplex LTC2380 for 2 channels. The datasheet doesn't mention anything about multiplexing, and I couldn't find specific information online.

I've also bought AD7641, and its datasheet has a section dedicated to using a MUX.

The IC I plan to use as mux is MAX4618, and required input BW is 250KHz per channel. Is it fine to use LTC2380 in this case? Any downsides about using it instead of AD7641?

Also, the signal to be acquired is going to be the output of a preamplifier, passing through a (less than 1m long) cable, and it's bipolar. What is the best practice for this? I'd like to make use of the fact the converter is differential to reduce cable noise, but according to the datasheets, none of them can accept bipolar signals directly.

Best regards,

Vitor.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.