Hi all,
AD7768 has two digital filters sinc and a wideband filter which is should use for analog signals.
Thanks & Regards,
Siva.
AD7768
Recommended for New Designs
The AD7768/AD7768-4 are 8-channel and 4-channel 24-bit, simultaneous sampling, sigma-delta (Σ-Δ) analog-to-digital converters (ADCs) with power scaling...
Datasheet
AD7768 on Analog.com
Hi all,
AD7768 has two digital filters sinc and a wideband filter which is should use for analog signals.
Thanks & Regards,
Siva.
Hi,
The answer to this question depends on input bandwidth and speed of the conversion versus the desired power mode or resolution. Sinc5 is ideal for low bandwidth signal and it has better noise peformance and lower power consumption. But if a wider bandwidth and faster ODR is required you can use the other filter type. The bandwidth for each filter is shown here below.
Sinc5 low latency filter, −3 dB at 0.204 × ODR
Wideband low ripple filter, −3 dB at 0.433 × ODR
So it really depends on your required specs and conditions.
Thanks,
Jellenie