Post Go back to editing

AD7606C-16: The relationship between SCLK frequency and sampling rate

Dear Technical Support Team,

Is there relationship between SCLK frequency and sampling rate?

According to the datasheet, 60MHz(VDRIVE > 2.7 V) is the max frequency.

My microcontroller is max 16MHz for SCLK. 

My target is over 200ksps and 8ch simultaneous sampling. SPI is serial interface.

Best Regards,

ttd



Add "SPI I/F is serial mode."
[edited by: ttd at 11:10 PM (GMT -4) on 25 May 2021]
Parents Reply Children
No Data