Hi,
we are working ADAS3022EDZ Eval board to communicate SPI through Arduino board. please help me
ADAS3022
Production
The ADAS3022 is a complete 16-bit, 1 MSPS, successive approximation–based analog-to-digital data acquisition system, which is manufactured on Analog Devices...
Datasheet
ADAS3022 on Analog.com
Hi,
we are working ADAS3022EDZ Eval board to communicate SPI through Arduino board. please help me
bakyaraj,
As previously requested we will need additional information regarding how you've modified the evaluation board to connect your controller, the code you are currently using and any physical result data you can share to help us diagnose you problem.
Sean
hi
Could please share SPI to All channel working (differential and Single end and Sequence).
That will help us our project.
Evaluation have 5 boards Same issue.
Project very critical please help me.
bakyaraj,
If REFIN = 0 volts on the evaluation board something is potentially wrong with your setup.
Please try running just the following small portion of your code.
1) Power up the board.
2) PD = 0.
3) Pulse Reset.
This should put the device in the default state. Please remeasure
REFIN, REF1/2, ACAP, DCAP and RCAP. If any of these are not their expected values then check
1) the PD pin is truly cleared.
2) RESET is not asserted
3) If the states of PD and RESET are correct verify that you have power applied to VIO, AVDD, DVDD.
Until we can get the reference to start-up there is no point playing with the interface as we can't be sure the part is correctly biased.
If you see the reference come up after running this short sequence try the following.
Send three conversion sequences consisting of.
1) A conversion pulse
2) A serial transaction of 16 clocks (Just send 0's. Don't try to update the interface)
On the final conversion sequence extend the number of clocks to 32 clocks (send two words) and verify the contents that comes out of SDO = 0x7FFF which is the default. If this works then we can be reasonably confident the setup is working.
Next try repeating the sequence of three short conversions this time inserting your 0xF7FE command. You should read back 0x77FE from the part after the third conversion with the extended readback.
If you are still having trouble after this let me know and I will try to get a setup working in the lab on Monday to show you everything working. The other thing to try (assuming you have a CED controller board) is to revert one board and verify it works yourself just to be sure the hardware is not in someway damaged.
Sean
Thanks Reply.....
Could you please share your working hardware result. Its also help us
We are following the above the procedure. we have attached timing end of 0x77FE
bakyaraj,
So inferring from the data you provided I'm assuming.
I'm assuming however that you still are not getting results that make sense to you.
Are you still seeing results similar to what you reported previously?
Sean
bakyaraj,
I will work on getting these plots for you this morning.
Sean
Hi,
we are try to read result differential input measurement (0xF7FE) configuration to All channel result
first case:
IN0 = -5v
IN1 = 5v
IN2 = open
IN3 = open
IN4 = open
IN5 = open
IN6 =open
IN7 = open
Second Case:
IN0 = -5v
IN1 = 5v
IN2 = open
IN3 = open
IN4 = open
IN5 = open
IN6 = -5v
IN7 = +5v
Com = 0V
bakyraj,
First of all you should not leave any of the inputs floating while converting. Please tie them to ground or some other stable voltage.
Second here are the timing patterns you requested with screen shots from the evaluation software showing everything working in the desired configurations.
Differential Channels Configuration (4 channels)
Conversion Results Differential Mode (500 Ksps, Normal Mode), 0V Differential Input
Diff to COM (8 Channel Mode)
Configuration
Results:
Very Thanks, i will working and update you
Very Thanks, i will working and update you
one Question,
1.CFG to how many 0000 to write the SPI
2.Continuous Conversion process don't need any RESET and PD
bakyaraj,
During configuration I write the configuration onto MOSI (SDI) on the first conversion serial transfer and then execute two more conversions with data accesses with 0x0000 passed to the device such that no further updates to the configuration word are requested. This ensures that the NEXT conversion started will give me the result (in this case) of channel 0-1, followed by the difference of channels 2-3, then channels 4-5, channels 6-7 and so on as I loop the data capture.
During data capture I always send 0x0000 to avoid updating the configuration word.
In all my setups RESET = 0, PD = 0 so I did not capture them.
Sean
Sk,
Thanks Reply.
I will testing and update you.
SK,
Differential and Single end both are working fine.
Very Thanks lot....