Hello,
I'm looking to convert two analog input signals (0-10V) to an single RS232 output.
If anyone can recommend a product, I would greatly appreciate it.
Thanks!
Hello,
I'm looking to convert two analog input signals (0-10V) to an single RS232 output.
If anyone can recommend a product, I would greatly appreciate it.
Thanks!
Hi,
We have a lot of Precision ADCs that can convert 0 to 10V but most of our output interface are either in serial or parallel interface, Can ypu provide more details regarding your application specs requirements, block diagram etc.? In this way we can narrow down the selection. But I have attached here the link to our selection page that you may find helpful.
Selection Table for Precision A/D Converters | Parametric Search | Analog Devices
I would also suggest to ask someone from (+) Q&A - Interface and Isolation - EngineerZone (analog.com) regarding the RS232 drivers.
Thanks,
Jellenie
Hi Jglad,
if I understood your question correctly, you have two analog input signals ranging from 0 to 10 V each that you want to convert to a single RS232 output. Most of the RS232 transceivers we have, accept ttl/cmos input levels and convert them to an RS232 output signal. You would probably need an ADC / convert it to ttl/cmos levels first. We have isolated as well as non isolated RS232 transceivers. Galvanically isolated modules in general, break ground loops and provide a convenient, self-powered, isolated, low EMI solution that drastically reduces component count and design complexity. RS-232 / RS-422 / RS-485 / RS-562 | Analog Devices. More explanation on what you're trying to do will help us point you to a specific product.
Regards,
Naveen
Thanks!
Thanks!