Post Go back to editing

AD7329 reference voltage

Hi all!

I'd like to use the AD7329 in my design.
  From what I understand, a 2.5V reference can be used to measure up to ±10V and a 3V reference can be used to measure ±12V at the analog input pins.
  Reading through the datasheet, it's not clear to me what reference voltage is needed when I want to be able to measure ±16.5V at the analog input pins.

Thanks in advance!

Parents
  • HI, 

    Just to add. May I know what is your application, and is the ±16.5V your max input range? If you can give us your specific requirements we can recommend an ADC that will suit your requirements. You may also want to consider using AD411x (AD4111, AD4112, AD4114,AD4115). The part have specified accuracy at  +/-10V but can be functional up to +/-20V with 2.5Vref and a single 5V supply. Please see the datasheet for your reference. 

    Thanks,

    Jellenie

Reply
  • HI, 

    Just to add. May I know what is your application, and is the ±16.5V your max input range? If you can give us your specific requirements we can recommend an ADC that will suit your requirements. You may also want to consider using AD411x (AD4111, AD4112, AD4114,AD4115). The part have specified accuracy at  +/-10V but can be functional up to +/-20V with 2.5Vref and a single 5V supply. Please see the datasheet for your reference. 

    Thanks,

    Jellenie

Children
  • Hi,

    Thanks for your reply! Slight smile

    I'm measuring an array of 12V industrial analog sensors. The output of these is up to 12V, but the system is very noisy and therefore has peaks of up to 15-16V. As I need to be aware of these peaks as well, I don't want to filter these out before it goes into the ADC.

    I already bought a batch of the AD7329 IC's, so unless this IC is not usable for what I'm trying to do then I would rather not switch to a different IC.

    Thanks,

    eutim

  • Hi, 

    Thanks for the details. With voltage of 3V, the range for +/-10V mode will be +/-12V. So the part can work with your max input range however any input voltage beyond this range will just result in a full scale code. 

    Thanks,

    Jellenie