Post Go back to editing

ad5941 ocp measurement

Thread Summary

The user asks how to measure the open circuit potential (OCP) between RE and WE (or AINx) before EIS measurements using the AD5941. The final answer suggests changing the ADC mux inputs in the AppIMPSeqCfgGen() function to monitor the OCP with RE0 and SE0 open-circuited. For the AD5940_BATZ EVAL board, which lacks a RE connection, the solution involves configuring the ADC mux to measure the potential drop across AIN2 and AIN3.
AI Generated Content

Hi, How can ad5941 measure the open circuit potential(OCP) between RE and WE(or AINx) before EIS measurement?

Parents
  • Hi,

    You may change the ADC mux inputs as shown below and monitor the output keeping RE0 and SE0 Open circuited.

    In AppIMPSeqCfgGen() function,

    dsp_cfg.ADCBaseCfg.ADCMuxN = ADCMUXN_HSTIA_N; //Replace with ADCMUXN_AIN3. You may short RE0 to AIN3.
    dsp_cfg.ADCBaseCfg.ADCMuxP = ADCMUXP_HSTIA_P; //Replace with ADCMUXP_VSE0

  • Thank you so much for your continued help. I'm using the AD5940_Impedance example measures 700 Ω pure resistance with Nucleo-f411, but the result is wrong when the measurement frequency is lower than 100Hz. I don't need to wait to get the result, even if the excitation frequency is 0.1Hz, of course, the result is wrong. I guess it's the sampling frequency, but compared with the AD5940_BATImpedance example I still can't find the solution.

  • Hi,

    Below is the open circuit result obtained by measuring current input by running AD5940_BATImpedance example:

    Hello AD5940-Build Time:00:28:16
    i: 1 Freq: 1.00 RcalVolt:(-4.000000,5.000000)
    i: 2 Freq: 1.44 RcalVolt:(0.000000,2.000000)
    i: 3 Freq: 2.07 RcalVolt:(0.000000,-2.000000)
    i: 4 Freq: 2.98 RcalVolt:(-2.000000,0.000000)
    i: 5 Freq: 4.28 RcalVolt:(-3.000000,-1.000000)
    i: 6 Freq: 6.16 RcalVolt:(2.000000,2.000000)
    i: 7 Freq: 8.86 RcalVolt:(-1.000000,-1.000000)
    i: 8 Freq: 12.74 RcalVolt:(2.000000,0.000000)
    i: 9 Freq: 18.33 RcalVolt:(-1.000000,-1.000000)
    i: 10 Freq: 26.37 RcalVolt:(1.000000,-2.000000)
    i: 11 Freq: 37.93 RcalVolt:(0.000000,0.000000)
    i: 12 Freq: 54.56 RcalVolt:(-1.000000,-1.000000)
    i: 13 Freq: 78.48 RcalVolt:(-2.000000,1.000000)
    i: 14 Freq: 112.88 RcalVolt:(0.000000,0.000000)
    i: 15 Freq: 162.38 RcalVolt:(0.000000,0.000000)
    i: 16 Freq: 233.57 RcalVolt:(0.000000,0.000000)
    i: 17 Freq: 335.98 RcalVolt:(0.000000,-1.000000)
    i: 18 Freq: 483.29 RcalVolt:(-5.000000,10.000000)
    i: 19 Freq: 695.19 RcalVolt:(7.000000,3.000000)
    i: 0 Freq: 1000.00 RcalVolt:(-1.000000,-4.000000)

    In AD5940-Impedance example,

    By setting

    pImpedanceCfg->ADCSinc3Osr = ADCSINC3OSR_5;//ADCSINC3OSR_2; and

    clk_cfg.HfOSC32MHzMode = bTRUE;//bFALSE;

    The following results are obtained from 20HZ to 100HZ. (with 700 Ohm resistor)

    Freq:19.05 RzMag: 692.232971 Ohm , RzPhase: 1.475751
    Freq:19.95 RzMag: 692.799744 Ohm , RzPhase: -1.111682
    Freq:20.89 RzMag: 680.045471 Ohm , RzPhase: -2.793056
    Freq:21.88 RzMag: 661.422974 Ohm , RzPhase: -3.216097
    Freq:22.91 RzMag: 645.959839 Ohm , RzPhase: -2.339729
    Freq:23.99 RzMag: 641.814575 Ohm , RzPhase: -0.642113
    Freq:25.12 RzMag: 651.756897 Ohm , RzPhase: 0.916017
    Freq:26.30 RzMag: 668.785034 Ohm , RzPhase: 1.602847
    Freq:27.54 RzMag: 685.240784 Ohm , RzPhase: 1.311895
    Freq:28.84 RzMag: 694.221558 Ohm , RzPhase: 0.339761
    Freq:30.20 RzMag: 692.621460 Ohm , RzPhase: -0.562610
    Freq:31.62 RzMag: 684.737183 Ohm , RzPhase: -0.894352
    Freq:33.11 RzMag: 678.146484 Ohm , RzPhase: -0.482382
    Freq:34.67 RzMag: 679.080505 Ohm , RzPhase: 0.215308
    Freq:36.31 RzMag: 686.552795 Ohm , RzPhase: 0.540739
    Freq:38.02 RzMag: 693.679321 Ohm , RzPhase: 0.280782
    Freq:39.81 RzMag: 694.289307 Ohm , RzPhase: -0.194708
    Freq:41.69 RzMag: 689.622375 Ohm , RzPhase: -0.371795
    Freq:43.65 RzMag: 687.199158 Ohm , RzPhase: -0.062749
    Freq:45.71 RzMag: 689.923523 Ohm , RzPhase: 0.250347
    Freq:47.86 RzMag: 694.028198 Ohm , RzPhase: 0.133161
    Freq:50.12 RzMag: 693.865723 Ohm , RzPhase: -0.177879
    Freq:52.48 RzMag: 691.126831 Ohm , RzPhase: -0.123374
    Freq:54.95 RzMag: 691.421021 Ohm , RzPhase: 0.137232
    Freq:57.54 RzMag: 693.953308 Ohm , RzPhase: 0.109119
    Freq:60.26 RzMag: 693.897888 Ohm , RzPhase: -0.116462
    Freq:63.10 RzMag: 692.540649 Ohm , RzPhase: -0.022710
    Freq:66.07 RzMag: 693.953796 Ohm , RzPhase: 0.082037
    Freq:69.18 RzMag: 694.391968 Ohm , RzPhase: -0.066963
    Freq:72.44 RzMag: 693.000854 Ohm , RzPhase: -0.005307
    Freq:75.86 RzMag: 693.917725 Ohm , RzPhase: 0.057995
    Freq:79.43 RzMag: 694.427185 Ohm , RzPhase: -0.043611
    Freq:83.18 RzMag: 693.465088 Ohm , RzPhase: -0.025996
    Freq:87.10 RzMag: 694.454224 Ohm , RzPhase: 0.043604
    Freq:91.20 RzMag: 693.962524 Ohm , RzPhase: -0.014548
    Freq:95.50 RzMag: 694.495117 Ohm , RzPhase: 0.010484
    Freq:100.00 RzMag: 694.465271 Ohm , RzPhase: -0.041118

    You may add 

    AD5940_AFEPwrBW(AFEPWR_LP, AFEBW_50KHZ)

    and Check for lower frequencies.

  • You may Update AFE in interrupt handler using function

    AppAMPRegModify(pBuff, &FifoCnt);   

    as shown below:

    int32_t AppIMPRegModify(int32_t * const pData, uint32_t *pDataCount)
    {
    HSLoopCfg_Type HsLoopCfg;
    DSPCfg_Type dsp_cfg;
    CLKCfg_Type clk_cfg;
    float nextfreq;
    uint32_t WaitClks;
    ClksCalInfo_Type clks_cal;
    FreqParams_Type freq_params;
    uint32_t SeqCmdBuff[2];
    uint32_t SRAMAddr = 0;;


    if(AppIMPCfg.NumOfData > 0)
    {
    AppIMPCfg.FifoDataCount += *pDataCount/4;
    if(AppIMPCfg.FifoDataCount >= AppIMPCfg.NumOfData)
    {
    AD5940_WUPTCtrl(bFALSE);
    return AD5940ERR_OK;
    }
    }
    if(AppIMPCfg.SweepCfg.SweepEn) /* Need to set new frequency and set power mode */
    {
    AD5940_WGFreqCtrlS(AppIMPCfg.SweepNextFreq, AppIMPCfg.SysClkFreq);
    }


    AppIMPCtrl(IMPCTRL_GETFREQ, &nextfreq);
    freq_params = AD5940_GetFreqParameters(nextfreq);

    if (nextfreq<0.11)
    {

    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<0.51)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<20)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_50KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<450)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;


    }
    else if(nextfreq<80000)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<=200000)
    {
    AppIMPCfg.PwrMod = AFEPWR_HP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    //clk_cfg.SysClkDiv = SYSCLKDIV_2;
    clk_cfg.HfOSC32MHzMode = bTRUE;

    AppIMPCfg.HsDacUpdateRate = 7;

    }

    HsLoopCfg.HsDacCfg.HsDacUpdateRate = AppIMPCfg.HsDacUpdateRate;
    dsp_cfg.ADCFilterCfg.ADCSinc2Osr = freq_params.ADCSinc2Osr;
    dsp_cfg.ADCFilterCfg.ADCSinc3Osr = freq_params.ADCSinc3Osr;
    dsp_cfg.DftCfg.DftNum =freq_params.DftNum;
    dsp_cfg.DftCfg.DftSrc = freq_params.DftSrc;

    AD5940_CLKCfg(&clk_cfg);
    AD5940_HSLoopCfgS(&HsLoopCfg);
    memset(&dsp_cfg.StatCfg, 0, sizeof(dsp_cfg.StatCfg));
    AD5940_DSPCfgS(&dsp_cfg);

    /* Step 3: Calculate clocks needed to get result to FIFO and update sequencer wait command */
    clks_cal.DataType = DATATYPE_DFT;
    clks_cal.DftSrc = freq_params.DftSrc;
    clks_cal.DataCount = 1L<<(freq_params.DftNum+2); /* 2^(DFTNUMBER+2) */
    clks_cal.ADCSinc2Osr = freq_params.ADCSinc2Osr;
    clks_cal.ADCSinc3Osr = freq_params.ADCSinc3Osr;
    clks_cal.ADCAvgNum = 0;
    clks_cal.RatioSys2AdcClk = AppIMPCfg.SysClkFreq/AppIMPCfg.AdcClkFreq;
    AD5940_ClksCalculate(&clks_cal, &WaitClks);

    /* Maximum number of clocks is 0x3FFFFFFF. More are needed if the frequency is low */
    if(WaitClks > 0x3FFFFFFF)
    {
    WaitClks /=2;
    SRAMAddr = AppIMPCfg.MeasureSeqInfo.SeqRamAddr;
    SeqCmdBuff[0] = SEQ_WAIT(WaitClks);
    AD5940_SEQCmdWrite(SRAMAddr+11, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+12, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+18, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+19, SeqCmdBuff, 1);
    }
    else
    {
    SRAMAddr = AppIMPCfg.MeasureSeqInfo.SeqRamAddr;
    SeqCmdBuff[0] = SEQ_WAIT(WaitClks);
    AD5940_SEQCmdWrite(SRAMAddr+11, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+18, SeqCmdBuff, 1);
    }

    if(AppIMPCfg.StopRequired == bTRUE)
    {
    AD5940_WUPTCtrl(bFALSE);
    return AD5940ERR_OK;
    }

    return AD5940ERR_OK;
    }

    You may refer to AppBIOZCheckFreq() in AD5940_BIOZ_2_Wire code 

    ad5940-examples/BIOZ-2Wire.c at master · analogdevicesinc/ad5940-examples · GitHub

Reply
  • You may Update AFE in interrupt handler using function

    AppAMPRegModify(pBuff, &FifoCnt);   

    as shown below:

    int32_t AppIMPRegModify(int32_t * const pData, uint32_t *pDataCount)
    {
    HSLoopCfg_Type HsLoopCfg;
    DSPCfg_Type dsp_cfg;
    CLKCfg_Type clk_cfg;
    float nextfreq;
    uint32_t WaitClks;
    ClksCalInfo_Type clks_cal;
    FreqParams_Type freq_params;
    uint32_t SeqCmdBuff[2];
    uint32_t SRAMAddr = 0;;


    if(AppIMPCfg.NumOfData > 0)
    {
    AppIMPCfg.FifoDataCount += *pDataCount/4;
    if(AppIMPCfg.FifoDataCount >= AppIMPCfg.NumOfData)
    {
    AD5940_WUPTCtrl(bFALSE);
    return AD5940ERR_OK;
    }
    }
    if(AppIMPCfg.SweepCfg.SweepEn) /* Need to set new frequency and set power mode */
    {
    AD5940_WGFreqCtrlS(AppIMPCfg.SweepNextFreq, AppIMPCfg.SysClkFreq);
    }


    AppIMPCtrl(IMPCTRL_GETFREQ, &nextfreq);
    freq_params = AD5940_GetFreqParameters(nextfreq);

    if (nextfreq<0.11)
    {

    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<0.51)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<20)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_50KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<450)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;


    }
    else if(nextfreq<80000)
    {
    AppIMPCfg.PwrMod = AFEPWR_LP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    AppIMPCfg.HsDacUpdateRate = 27;

    }
    else if(nextfreq<=200000)
    {
    AppIMPCfg.PwrMod = AFEPWR_HP;
    AD5940_AFEPwrBW(AppIMPCfg.PwrMod, AFEBW_250KHZ);
    //clk_cfg.SysClkDiv = SYSCLKDIV_2;
    clk_cfg.HfOSC32MHzMode = bTRUE;

    AppIMPCfg.HsDacUpdateRate = 7;

    }

    HsLoopCfg.HsDacCfg.HsDacUpdateRate = AppIMPCfg.HsDacUpdateRate;
    dsp_cfg.ADCFilterCfg.ADCSinc2Osr = freq_params.ADCSinc2Osr;
    dsp_cfg.ADCFilterCfg.ADCSinc3Osr = freq_params.ADCSinc3Osr;
    dsp_cfg.DftCfg.DftNum =freq_params.DftNum;
    dsp_cfg.DftCfg.DftSrc = freq_params.DftSrc;

    AD5940_CLKCfg(&clk_cfg);
    AD5940_HSLoopCfgS(&HsLoopCfg);
    memset(&dsp_cfg.StatCfg, 0, sizeof(dsp_cfg.StatCfg));
    AD5940_DSPCfgS(&dsp_cfg);

    /* Step 3: Calculate clocks needed to get result to FIFO and update sequencer wait command */
    clks_cal.DataType = DATATYPE_DFT;
    clks_cal.DftSrc = freq_params.DftSrc;
    clks_cal.DataCount = 1L<<(freq_params.DftNum+2); /* 2^(DFTNUMBER+2) */
    clks_cal.ADCSinc2Osr = freq_params.ADCSinc2Osr;
    clks_cal.ADCSinc3Osr = freq_params.ADCSinc3Osr;
    clks_cal.ADCAvgNum = 0;
    clks_cal.RatioSys2AdcClk = AppIMPCfg.SysClkFreq/AppIMPCfg.AdcClkFreq;
    AD5940_ClksCalculate(&clks_cal, &WaitClks);

    /* Maximum number of clocks is 0x3FFFFFFF. More are needed if the frequency is low */
    if(WaitClks > 0x3FFFFFFF)
    {
    WaitClks /=2;
    SRAMAddr = AppIMPCfg.MeasureSeqInfo.SeqRamAddr;
    SeqCmdBuff[0] = SEQ_WAIT(WaitClks);
    AD5940_SEQCmdWrite(SRAMAddr+11, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+12, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+18, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+19, SeqCmdBuff, 1);
    }
    else
    {
    SRAMAddr = AppIMPCfg.MeasureSeqInfo.SeqRamAddr;
    SeqCmdBuff[0] = SEQ_WAIT(WaitClks);
    AD5940_SEQCmdWrite(SRAMAddr+11, SeqCmdBuff, 1);
    AD5940_SEQCmdWrite(SRAMAddr+18, SeqCmdBuff, 1);
    }

    if(AppIMPCfg.StopRequired == bTRUE)
    {
    AD5940_WUPTCtrl(bFALSE);
    return AD5940ERR_OK;
    }

    return AD5940ERR_OK;
    }

    You may refer to AppBIOZCheckFreq() in AD5940_BIOZ_2_Wire code 

    ad5940-examples/BIOZ-2Wire.c at master · analogdevicesinc/ad5940-examples · GitHub

Children
No Data