Post Go back to editing

Diagnotsic mux value error of AD7606

Hello 

I am using the AD7606B to gather adc data. In order to run self test, i tried Dignostic Mux register.

Even though i tried to select 2.5V for input , the result was 10V that i calculated.

The output 10V code is 32767 when i selected 2.5V.

Other voltages are correct value. 

So what do i wrong?

Parents Reply
  • Hi

    I checked reference voltage is 2.5V. 

    So i think 10V code have to be around 32768 / 4. But the result is around 32767.

    Even though it is a diagnostic channel, there is too much difference in value.

    Have you set 0x12(00010010) value on 0x28 which is address of AD7606b register?

    Or is 32767 value right because of error?

Children