EVAL-AD5940BIOZ SensorPal COM port problem

I am facing problems using EVAL-AD5940BIOZ with SensorPal.

I have tried everything in this:
wiki.analog.com/.../help_and_support

and in this:
wiki.analog.com/.../adicup3029_hw_drivers

It seems to update Firmware inside the SensorPal, but there is a problem with COM Port communication, it says:
"Connection to target on was not established"
(I do disconnect and connect dev-kit before trying to connect after firmware update)

I have also tried to erase flash using CrossCore, but it does not work. When I try to erase it says:
"No autobaud response"

UPDATE:

I have tried to use IAR EW for ARM, but it did not work either: "Fatal error: Failed to connect to CPU"



UPDATE: I have tried to use IAR EW for ARM, but it did not work either: "Fatal error: Failed to connect to CPU"
[edited by: Povsel at 4:11 PM (GMT -5) on 10 Feb 2021]

Top Replies