Post Go back to editing

Custom design PCB AD7293 using SDP-B

Hello

I'am currently working with the AD7293 evaluation board and the SDP-B programmer, which works well.

Now I'am planning to design my own board and would like to use it with the SDP-B programmer and standard evaluation software in a first step.

Do I need to place the 24LC32 EEPROM on my PCB to work with the SDP-B and evaluation board? And what do I have to write into the EEPROM?

Thanks in advance

Regards

Samuel

Parents
  • Hi Samuel,

    You will need to use the 24LC32 EEPROM as this is how the evaluation software identifies the board. You will need to use the same address as on the EVAL-AD7923SDZ evaluation board i.e. 0x54. The schematic is in the user guide. 

    You will need to program the EEPROM with the AD7293.dat file. Save the below text file as a .dat file and you can then program that file to the EEPROM. 

    U   ADISDP  U  e`x    AD7293 Evaluation Board# AD7293 Evaluation Board Software

    Regards,

    Valerie

  • Hi Valerie

    Thank you for your fast reply, just one more question, can i program the EEPROM with the SDP-B? Or do I need a separat programmer?

    Regards

    Samuel

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.