Post Go back to editing

EXCITATION CURRENT SOURCES for LTC2984

Hi Team, 

How many EXCITATION CURRENT SOURCES are there in LTC2984?

Parents
  • Hi ,

        There are multiple configurable current sources (current DACs) in the LTC2984 - however, typically only one is active at a time based on the channel configuration. 

        Cases where more than one current source is active:

    1) Thermocouple open-circuit detect uses a separate current source  from the one used by the cold-junction compensation sensor (Thermistor, RTD, or Diode) - those are active at the same time during the conversion.

    2) 3-wire RTDs use two matched current sources applied simultaneously to cancel the effect of the sensor lead resistance.

    Hope this helps, 

    -Logan

  • Hi Logan,

    Thanks for the information.

    Typically only one is active at a time--> I understood this point.

    You told that, there are multiple current sources in LTC2984--> I just want to know how many configurable current sources are there in the device?

    For an example if I want to connect 3 types of RTD(PT500, PT100, PT1000) means I need to configure three different types of IDACs for each type. For this kind of purpose I am asking the number of configurable current sources.

Reply
  • Hi Logan,

    Thanks for the information.

    Typically only one is active at a time--> I understood this point.

    You told that, there are multiple current sources in LTC2984--> I just want to know how many configurable current sources are there in the device?

    For an example if I want to connect 3 types of RTD(PT500, PT100, PT1000) means I need to configure three different types of IDACs for each type. For this kind of purpose I am asking the number of configurable current sources.

Children