Hello
Customer would like to meet 16000rpm ( 266.6rps). Do you have any suggestion or comments for 12bit or 14 bit resolution that more suitable for this specification? It looks max rps of 12 bit and 14 bit should meet 266.6 rps. Thank you.
Xtal:8.192Mhz
Pole pair: 4
Speed: 16000rpm (266.6rps)
BR
Patrick
Patrick,
Can you comment on if the speed quoted already accounts for the speed multiplier of the pole pair (electrical speed) or if it is the mechanical speed of the monitored shaft? Also is there a requirement…
Your understanding of the electrical rotation multiplier is correct and we would expect that at maximum velocity the resolver would generate a signal equivalent to 32000 RPM or 533 RPS. For this…
If I understand your queries correctly you are asking if velocity, tracking rate, etc. scale linearly with the input clock. The answer is yes that is correct.. If I'm missing anything else let…