AD2S1210 resolution setting

Hello

             Customer would like to meet 16000rpm ( 266.6rps). Do you have any suggestion or comments for 12bit or 14 bit resolution that more suitable for this specification?  It looks max rps of 12 bit and 14 bit should meet 266.6 rps. Thank you. 

 

Xtal:8.192Mhz

Pole pair: 4

Speed: 16000rpm (266.6rps)

       

BR

Patrick

Parents Reply
  • Hello Sean

               Per end customer feedback for resolution, there is a little difference by resolution setting as below. It is not recommend 12 bit, 1000rps, CLKIN=8.192MHz for 4x resolver. It is recommend to use 12 bit 1250 rps , CLKIN=10.24MHz. Do you have comment it? Which resolution and CLKIN is correct for 4x resolver (16000 rpm) 

               Another question, do we have any related doc. to explain motor pole/resolver/RDC relationship and setting for reference? Thank you. 

    BR

    Patrick

Children
  • +1
    •  Analog Employees 
    on Nov 9, 2020 12:09 PM 2 months ago in reply to patrickchen@morrihan.com

    Patrick,

    My apologies as I looked back to the original post and I missed that this was a 4x resolver.   So yes at 4x with maximum rotational velocity of 16000rpm the AD2S1210 will need to be faster than 1000 rps that is natively available at 8.192MHz.   For this reason the customer will need to use a CLKIN = 10.24 MHz.

    With regards to the documentation you requested we don't have such a document to my knowledge.

    Sean

  • Hello Sean

                  1. Customer's max speed looks 64000RPM. But encoder read speed can not meet 64000 RMP, right? Has any suggestion for encoder ex : has feature to divide max 64000RPM....

                  2. While measure 160000 RPM via encoder interface, There are different  PWM width as below waveform, Is it normal? What is the root cause for this phenomenon? 

                      3. The encoder description looks less on datasheet. What is max RPM support by encoder? It looks has only resolution for setting, right? If any document of encoder description, it will be better. Thank you. 

    BR

    Patrick 

  • Hello Sean

                 Do you have update for above question? Thank you. 

    BR

    Patrick

  • +1
    •  Analog Employees 
    on Nov 17, 2020 12:58 PM 2 months ago in reply to patrickchen@morrihan.com
      1. Customer's max speed looks 64000RPM. But encoder read speed can not meet 64000 RMP, right? Has any suggestion for encoder ex : has feature to divide max 64000RPM....

    Patrick you have two choices with respect to the encoder output to extend the range.  Firstly if you have already increased the master clock rate of the device then the max rotational frequency also increases proportional to that change as it does in the position/velocity reading case.   Second, you could alternatively change the resolution to 10-bit mode and extend the maximum rotational velocity through the mode change.

        2. While measure 160000 RPM via encoder interface, There are different  PWM width as below waveform, Is it normal? What is the root cause for this phenomenon? 

    This appears to be related to velocity ripple in your system configuration.

                      3. The encoder description looks less on datasheet. What is max RPM support by encoder? It looks has only resolution for setting, right? If any document of encoder description, it will be better. Thank you. 

    The encoder description is very sparse in the datasheet but you can assume the same dynamics for all resolution modes as with the primary data-path as they share the same source.  We are actually in the process of reviewing our training collateral for this product family and this will be valuable feedback to help us improve the support for this product.

  • Hello Sean

                For velocity ripple issue to cause encoder different pulse width, customer testing it on Hill and environment should be clean. . But while above 40000RPM speed, encoder signal will happen this issue. Do you have any suggestion for it? Thank you.  

    Speed: 40000RPM

    Ch2: AD2S1210  Sin

    Ch3: AD2S1210 Encoder A

    BR

    Patrick