AD2S1210 resolution setting

Hello

             Customer would like to meet 16000rpm ( 266.6rps). Do you have any suggestion or comments for 12bit or 14 bit resolution that more suitable for this specification?  It looks max rps of 12 bit and 14 bit should meet 266.6 rps. Thank you. 

 

Xtal:8.192Mhz

Pole pair: 4

Speed: 16000rpm (266.6rps)

       

BR

Patrick

Parents Reply Children
  • Hello Sean

                 We see many electrical specification on 8.192MHz. Could we know why don't use 10.24MHz CLKIN for electrical specification or by your opinion 10.24MHz CLKIN is more suitable than 8.192MHz CLKIN? Thank you.

    BR

    Patrick    

  • +1
    •  Analog Employees 
    on Oct 30, 2020 10:56 AM 2 months ago in reply to patrickchen@morrihan.com

    Patrick,

    Per the specification table 

    All performance is guaranteed for the entire valid clock range unless otherwise noted.   In the specification table where most often we see the specific CLKIN selection noted is to emphasize the linear relationship between the CLK and a specific parameter such as BANDWIDTH or TRACKING RATE. 

    Sean

  • Hello Sean

               Per end customer feedback for resolution, there is a little difference by resolution setting as below. It is not recommend 12 bit, 1000rps, CLKIN=8.192MHz for 4x resolver. It is recommend to use 12 bit 1250 rps , CLKIN=10.24MHz. Do you have comment it? Which resolution and CLKIN is correct for 4x resolver (16000 rpm) 

               Another question, do we have any related doc. to explain motor pole/resolver/RDC relationship and setting for reference? Thank you. 

    BR

    Patrick

  • +1
    •  Analog Employees 
    on Nov 9, 2020 12:09 PM 2 months ago in reply to patrickchen@morrihan.com

    Patrick,

    My apologies as I looked back to the original post and I missed that this was a 4x resolver.   So yes at 4x with maximum rotational velocity of 16000rpm the AD2S1210 will need to be faster than 1000 rps that is natively available at 8.192MHz.   For this reason the customer will need to use a CLKIN = 10.24 MHz.

    With regards to the documentation you requested we don't have such a document to my knowledge.

    Sean

  • Hello Sean

                  1. Customer's max speed looks 64000RPM. But encoder read speed can not meet 64000 RMP, right? Has any suggestion for encoder ex : has feature to divide max 64000RPM....

                  2. While measure 160000 RPM via encoder interface, There are different  PWM width as below waveform, Is it normal? What is the root cause for this phenomenon? 

                      3. The encoder description looks less on datasheet. What is max RPM support by encoder? It looks has only resolution for setting, right? If any document of encoder description, it will be better. Thank you. 

    BR

    Patrick