Hello
Customer would like to meet 16000rpm ( 266.6rps). Do you have any suggestion or comments for 12bit or 14 bit resolution that more suitable for this specification? It looks max rps of 12 bit and 14 bit should meet 266.6 rps. Thank you.
Xtal:8.192Mhz
Pole pair: 4
Speed: 16000rpm (266.6rps)
BR
Patrick
Patrick,
Can you comment on if the speed quoted already accounts for the speed multiplier of the pole pair (electrical speed) or if it is the mechanical speed of the monitored shaft? Also is there a requirement…
Your understanding of the electrical rotation multiplier is correct and we would expect that at maximum velocity the resolver would generate a signal equivalent to 32000 RPM or 533 RPS. For this…
If I understand your queries correctly you are asking if velocity, tracking rate, etc. scale linearly with the input clock. The answer is yes that is correct.. If I'm missing anything else let…
Can you comment on if the speed quoted already accounts for the speed multiplier of the pole pair (electrical speed) or if it is the mechanical speed of the monitored shaft? Also is there a requirement for overspeed indication?
Thanks
Sean
Hello Sean
The speed ex 16000rpm should be mechanical speed. Customer's motor is 4 Pole-Pairs. the resolver is 2 Pole-Pairs. So at motor run a cycle, we should get SIN/COS speed become double, is it correct? Please refer to below waveform. above pic is 4 Pole-Pairs, below pic is 2 Pole Pairs.
if correct, the motor run one cycle, the resolver get speed from 16000 rpm to 32000 rpm. If consider resolution setting, we need to depend 32000 rpm for our resolution setting, right?
It is a little urgent, so need your help to clarify above questions, Thank you.
BRPatrick
Your understanding of the electrical rotation multiplier is correct and we would expect that at maximum velocity the resolver would generate a signal equivalent to 32000 RPM or 533 RPS. For this reason I would recommend the customer select 12-bit resolution mode.
Thank you for your suppport. Thanks.
We see our specification most used CLKIN=8.192MHz. Customer request Velocity LSB, tracking rate and other specification depend on CLKIN=10.24 MHz. Do we related specification of 10.24MHz to customer?
BTW, the velocity LSB and tracking rate looks linear to CLKIN. If 12 bit resolution (0.488 rps), it will become to 0.61 rps, right? Thank you.
If I understand your queries correctly you are asking if velocity, tracking rate, etc. scale linearly with the input clock. The answer is yes that is correct.. If I'm missing anything else let me know.