Hi
AD7124-8 datasheet page 7, Normal Mode Rejection use Sinc4 Filter & Internal Clock is 98dB(min),
My Setting
Best Regards,
Eric Lo
Hi Eric,
Actually if you look at the specs, the datasheet is specified as a minimum value which means that the actual value is guaranteed to not be lower than that but it can go higher than that. I think…
Actually if you look at the specs, the datasheet is specified as a minimum value which means that the actual value is guaranteed to not be lower than that but it can go higher than that. I think the virtual eval is usually based from the typical spec performance but it is not specified in the datasheet.
Thanks,
Jellenie