AD7147P-1 -> USB Communication failed

Hi Sir

I use J2 to connect to an external PCB board, which can read AD7147-1 normally
But after changing to AD7147P-1
Execute CDC Converter and read greph, it shows **USB communication failed**

AD7147-1 => AD7147ACPZ-1500RL7
AD7147P-1 => AD7147PACPZ-1500PL7

1. Are AD7147-1 and AD7147P-1 pin to pin?
2. Is the communication interface of AD7147P-1 I2C?

PC link to EVB

Open EVAL-AD7147 Software

Register Configuration

=>CDC Converter=>Read Graph

  • 0
    •  Analog Employees 
    on Oct 22, 2020 3:30 AM 1 month ago

    AD7147-1 and AD7147P-1 are pin-to-pin complaint and both have I2C interfaces.

    Please provide more details.

    1. Have you replaced the parts on the same board?

    2. Did you check whether the new part has been soldered properly without any shorts or opens on any pads?

    3. Is the new part taking adequate current on the device supply after power-up?

  • AD7147-1 and AD7147P-1 are both pin-to-pin complaints, and both have an I2C interface.

    Please provide more details.

    1. Have you replaced the parts on the same board?
    Replace two AD7147Ps without modifying other parts

    2. Have you checked whether the new parts are soldered correctly, whether there are no short circuits or open pads?
    Yes, I check every pin with a magnifying glass

    3. After power on, does the new component get enough current on the equipment power supply?
    Yes, I use EVB's Vdrive to provide 3.3V

  • Hi Sir

    Excuse me, is there any update on this issue?

  • 0
    •  Analog Employees 
    on Nov 3, 2020 2:16 PM 28 days ago in reply to justin_322

    Hi Justin,

    The '-1' and 'P-1' versions have the same pin-outs and both are I2C parts.

    The only thing I can think of  (if it's not a soldering issue) is if the Device ID register contents are different (i.e. the Device ID/revision number may be different). I believe the GUI reads the Device ID reg and if it doesn't get back the value it expects then it gives the USB error. Can you 'tap into' the I2C lines and read that register directly with some I2C reader (this would also tell you if the part is 'alive'?  I did a quick search on our depository and unfortunately because the GUI is very old, it doesn't look like we have the source code for that GUI if the Device ID/revision is different.

    Regards,

    Dave