Configuration for universal analog input in AD7124_8

Hi,

!)I want to use AD7124_8 for universal analog input. So that I can connect channel number RTD or TC or 4-20mA or 0-10V.Is that possible with Ad7124_8?

2) AD7124 ADC 8 channel differential input is there so that can use channel one for RTD  application, Channel two for Thermocouple application,channel three for 4-20mA application, and channel four 0-10v application. So is that possible to configure like this way in AD7124_8?