Need information on AD976 Ain of >+/-10V

I need a better understanding of the +/-25V maximum input limit specified in the device.  How much current is allowed through the protection mechanism and what if the applied voltage is somewhere between +10V and +25V, for example 13.2V? will i be able to stay in that range indefinite and be over-scaled? or will i damage that AD976B. it does accept +/- 10V as typical but no max or min limts... other than absolute at +/-25V