Post Go back to editing

How do I interface to multiple AD719x ADCs over the same serial interface ?

Thread Summary

The user asked how to interface multiple AD719x ADCs over a single serial interface. The solution involves using a decoder to control the /CS (chip select) lines of the ADCs, ensuring only one ADC drives the DOUT line at a time. The AD719x can be synchronized using the SYNC pin to manage the /RDY signals, allowing data to be read from all ADCs without loss, provided the microcontroller can read data quickly enough without violating the 5 MHz SCLK frequency limit. For channel switching, refer to application note AN-1084.
AI Generated Content

How do I interface to multiple AD719x ADCs over the same serial interface ?

Parents Reply Children
No Data