On the AD779x, if a conversion is not read and the next conversion is completed, how long does DOUT/RDY go high ?
AD7796
Production
The AD7796/AD7797 are complete, analog front ends for high
precision, bridge sensor applications such as weigh scales. The
AD7796/AD7797 contain a S-?...
Datasheet
AD7796 on Analog.com
AD7792
Production
The AD7792/AD7793 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7792/AD7793 contain a low noise...
Datasheet
AD7792 on Analog.com
AD7794
Production
The AD7794/AD7795 are low power, low noise, complete analog front ends for high precision measurement applications. They contain a low noise, 24-/16-bit...
Datasheet
AD7794 on Analog.com
AD7793
Production
The AD7792/AD7793 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7792/AD7793 contain a low noise...
Datasheet
AD7793 on Analog.com
AD7797
Production
The AD7796/AD7797 are complete, analog front ends for high
precision, bridge sensor applications such as weigh scales. The
AD7796/AD7797 contain a S-?...
Datasheet
AD7797 on Analog.com
AD7799
Production
The AD7798/AD7799 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7798/AD7799 contains a low noise...
Datasheet
AD7799 on Analog.com
AD7798
Production
The AD7798 / AD7799 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7798 / AD7799 contains a low...
Datasheet
AD7798 on Analog.com
AD7795
Production
The AD7794/AD7795 are low power, low noise, complete analog front ends for high precision measurement applications. They contain a low noise, 24-/16-bit...
Datasheet
AD7795 on Analog.com
On the AD779x, if a conversion is not read and the next conversion is completed, how long does DOUT/RDY go high ?
The DOUT/RDY pin goes high for approximately 0.8 ms. During this time, the data register is updated with the new conversion data so the user should not attempt to read the data register.