When single conversion mode is used on the AD779x, can CS be taken high after the single conversion is initiated ?
AD7796
Production
The AD7796/AD7797 are complete, analog front ends for high
precision, bridge sensor applications such as weigh scales. The
AD7796/AD7797 contain a Σ-âˆ...
Datasheet
AD7796 on Analog.com
AD7792
Production
The AD7792/AD7793Â are low power, low noise, complete analog front ends for high precision measurement applications. The AD7792/AD7793 contain a low noise...
Datasheet
AD7792 on Analog.com
AD7794
Production
The AD7794/AD7795 are low power, low noise, complete analog front ends for high precision measurement applications. They contain a low noise, 24-/16-bit...
Datasheet
AD7794 on Analog.com
AD7793
Production
The AD7792/AD7793 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7792/AD7793 contain a low noise...
Datasheet
AD7793 on Analog.com
AD7797
Production
The AD7796/AD7797 are complete, analog front ends for high
precision, bridge sensor applications such as weigh scales. The
AD7796/AD7797 contain a Σ-âˆ...
Datasheet
AD7797 on Analog.com
AD7799
Production
The AD7798/AD7799 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7798/AD7799 contains a low noise...
Datasheet
AD7799 on Analog.com
AD7798
Production
The AD7798 /Â AD7799 are low power, low noise, complete analog front ends for high precision measurement applications. The AD7798 / AD7799 contains a low...
Datasheet
AD7798 on Analog.com
AD7795
Production
The AD7794/AD7795 are low power, low noise, complete analog front ends for high precision measurement applications. They contain a low noise, 24-/16-bit...
Datasheet
AD7795 on Analog.com
When single conversion mode is used on the AD779x, can CS be taken high after the single conversion is initiated ?
The serial interface is independent of the sampling process. So, once the single conversion is initiated, the AD779x will power up and perform the single conversion irrespective of the CS polarity. So, the user could take CS low, initiate the single conversion, and then take CS high again. When the conversion is complete, CS can be taken low to read the conversion and another single conversion can be started if required. When CS is taken high, the DOUT/RDY pin is tristated. Therefore, the DOUT/RDY pin will not indicate the end of the conversion. The user can determine the end of the conversion by reading the status register. Alternatively, the conversion time could be timed out by the microcontroller clock.