Post Go back to editing

Vinh/Vinl of AD7476A and AD7476B

Hello,

I have a question about logic voltage of AD7476A and AD7476B.

http://www.analog.com/en/analog-to-digital-converters/ad-converters/ad7476/products/product.html

Pls tell me the Vinh & Vinl when using VDD = 2.5V.

The data-sheet does not describe it. Pls refer to page3.

It would be greatly appreciated if advice could be gotten.

Best Regards,

  • Hello,

    Unfortunately we haven't specified Vinh and Vinl specifications at VDD of 2.5 V but please be aware that these are CMOS logic voltage thresholds therefore:

    At 2.5 V VDD the logic output specifications won't change therfore Voh and Vol are VDD-0.2 and 0.4 V respectively.

    Logic inputs, Vinl should be 0.4 V and Vinh around 1.8 V - 2.0 V.

    This device was successfully connected to the FPGA device supplied with 2.5 V without any difficulties.

    Regards,

    Jakub.

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin