Post Go back to editing

Daisy chain AD7706

Is it possible to daisy chain the AD7706?  If not, can anyone recommend a 16bit ADC that can be, preferably in a DIL package?

I have an application that requires over 50 ADCs, with 50 or 60 readings per second, so daisy chaining them would make it easy for me.  I also use the AD7710 a lot, knowing if that to can be daisy chained to would be useful.

Parents
  • Thanks Rob.

    The AD977 looks like it will do the job.  With the number of ADCs on the board I'd prefer to have them in DIL sockets, so if one goes it can be replaced.  As its a one off project the age of the component is not important.  The AD7980 also looks good, but I'd have to mount them on daughter boards.  No need for an evaluation board, I'll just buy a couple from Farnell.

    The project needs to measure 64, or possibly 128, potentials at 50 or 60 readings per second, so we can filter mains noise.  The potential will be bi-polar, but conditioning for a uni-polar ADC would be possible.  Great accuracy is not needed, but I chose 16 bit because its two bytes exactly so no wasted bits.  I'll be using a dsPIC to read the ADCs and send the data to the PC.

Reply
  • Thanks Rob.

    The AD977 looks like it will do the job.  With the number of ADCs on the board I'd prefer to have them in DIL sockets, so if one goes it can be replaced.  As its a one off project the age of the component is not important.  The AD7980 also looks good, but I'd have to mount them on daughter boards.  No need for an evaluation board, I'll just buy a couple from Farnell.

    The project needs to measure 64, or possibly 128, potentials at 50 or 60 readings per second, so we can filter mains noise.  The potential will be bi-polar, but conditioning for a uni-polar ADC would be possible.  Great accuracy is not needed, but I chose 16 bit because its two bytes exactly so no wasted bits.  I'll be using a dsPIC to read the ADCs and send the data to the PC.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.