Problem of AD7908.

Hi ,

I use the AD7908 and the current sensor IC "MAX4073T" without any OP between current sensor output and Vin of AD7908.

In some case, the output of current sensor will be 0.4V, but there is a 3.6V rising due to the reverse current of ADC.

I put an 1M ohm resistor between two IC's to reduce the reverse current temporarily.

Is there any possible error that may happen in my circuit?

Thanks a lot,
Stan

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:29 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:29 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data