Post Go back to editing

About AD7690 ADC

Dear Sir/Madam,

     We are using the AD7690 High speed ADC for our weigh scale application. The ADC input is giving from the Loadcell. In that we using the ARM7 processor.

In that, we developed the firmware in c language to read the digital counts from AD7690 .

Please see the following conditions which we made in hardware side,

*We are using the CS mode, with 3-wire communication(CNV,SDO and Sclk) without busy indicator.

*We connected the VIO to SDI continuously (5v).

*But, the problem was, we were not receiving Any data from the ADC. We think that there might be a problem within our software program.

     Please give us, desired flow to develope the software for this ADC. Please give us any sample code to develope our application with AD7690.

Thanks and Regards,

Vijay.

Parents
  • Hi Vijay,

    Sorry for the late reply. The AD7690 is a fully differential input. This means the positive and negative inputs must be antiphase around the common mode voltage Vref/2, the IN- pin cannot be tied to ground for proper operation. Is 18 bit performance important to you? If so you can use an amp such as the ADA4941 to perform singe ended to differential conversion.

    Best Rgds,

    Alan

Reply
  • Hi Vijay,

    Sorry for the late reply. The AD7690 is a fully differential input. This means the positive and negative inputs must be antiphase around the common mode voltage Vref/2, the IN- pin cannot be tied to ground for proper operation. Is 18 bit performance important to you? If so you can use an amp such as the ADA4941 to perform singe ended to differential conversion.

    Best Rgds,

    Alan

Children
No Data