Questions about AD7682

Hi,
   I am using AD7682 to make a data aquisition system.
   I connected the COM(pin10) to GND and used the internal reference 2.5V.
   But when the amplitude of the input sinewave exceed about 1.2V, half of the reference voltage, it seemed that the waveform ploted according to the converted result not exactly the right.
   Why it performs like this?
   By the way, the input signal composed of about 600mV DC offset and a sinewave about 600-700mV peak to peak?
   When I used the internal 4.096V reference, should the input voltage below about 2V? Or it could be 4.096V?
   Thank you!

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:32 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:32 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data