For the AD7782, how do you set the MODE pin to achieve MASTER and SLAVE?
The current version of the datasheet posted on the web site (http://www.analog.com/en/analog-to-digital-converters/ad-converters/ad7782/products/product.html, version 2001 rev0), says the following:
-page 5 in caption for Figure 2: SLAVE MODE IS SELECTED BY TYING THE MODE PIN LOW, WHILE MASTER MODE IS SELECTED BY TYING THE MODE PIN HIGH.
-page 6 in notes for MODE pin: The MODE pin selects master or slave mode of operation. When MODE = 0, the AD7782 operates in master mode while the AD7782 is configured for slave mode when MODE = 1.
These are contradictory statements. Does anyone know the correct option?