Post Go back to editing

AD7787 not working

Hi people!

I just bought an ad7787 and I cant get it running.I have read the code you attached but Im having some troubles understanding it, probably because my knowledge about C is not that good. Anyway, I have connected the device to a atmega1281 that I have used a lot, by the SPI. I can see in my oscilloscope that when I send my commands to comm register the sclk and cs lines are correct but the data is not.

Then I try to read the data register but the value I get is 0x80 no matter what value is on the AIN2.

I attached my scheme and my code.

Cheers,

Dan.

/*

* Prueba del ADC con el mote

* Created: 30/07/2012 10:05:44

* Author: Daniel

*/

#include <avr/io.h>

#include <avr/interrupt.h>

#include <avr/power.h>

#include <util/delay.h>

#define F_CPU 4000000UL //4 MHz

#include <avr/sfr_defs.h>

//Variables globales

unsigned char data=0x3D,aux2,aux4;

int adc=0x00;

//Mis funciones

void SPI_MasterInit(void);

void _delay_ms (double __ms);

writetoreg(unsigned char data);

int readfromreg();

int main(void)

{

//Configurar puertos e inicializar

             SPI_MasterInit();

             sei();

            

       while(1)

    {

             data=0x3D; //continuous mode - ain2(single ended)

             writetoreg(data); //write to comm register

             adc = readfromreg();//read data

             }

}

void SPI_MasterInit(void)

{

/* Set MOSI,SS and SCK output, all others input */

DDRB = (1<<DDB1)|(1<<DDB2)|(1<<DDB0)|(1<<DDB4)|(1<<DDB5);

PORTB = (1<<PB0)|(1<<PB4)|(1<<PB2);//fsync disp1

/* Enable SPI, Master, set clock rate fck/16 , MSB first*/

SPCR = (1<<SPE)|(1<<MSTR)|(1<<SPR0)|(0<<DORD)|(1<<CPOL)|(0<<CPHA);

}

writetoreg(unsigned char data)

{

       PORTB = (0<<PB0)|(1<<PB4)|(1<<PB5);//cs low

             // Start transmission

             SPDR = data;

             // Wait for transmission complete

             while(!(SPSR & (1<<SPIF)));

             aux2 = SPSR;

       PORTB = (1<<PB0)|(1<<PB4)|(1<<PB5);// cs high

}

int readfromreg()

{

       PORTB = (0<<PB0)|(1<<PB4)|(1<<PB5);//cs low

       // Start transmission

       while(!(SPSR & (1<<SPIF)));

       adc = SPSR;

       PORTB = (1<<PB0)|(1<<PB4)|(1<<PB5);// cs high

       return adc;

}     

Parents Reply Children
No Data