AD7682 Configuration problem

Hello,

I'm using the AD7682 ADC with a msp430 talking spi.  After a power I'm trying to configure the device but the configuration I'm reading back does not match the one I'm sending.  Here's what I'm sending:

0xFF70 (Which is 0x3FDC bit shifted left by 2 because of the 14 bit config register)

So I'm trying to set the following parameters:

bits

13          Overwrite Config

12:10     Unipolar, INx referenced to GND

9:7         IN3 is last conversion

6           Full BW

5:3        External reference, internal buffer, temp enabled

2:1        Scan 0:3 then temp

0           read back current config at the end of data

but this is what I'm receiving back from the device

0xE2E3

13       Overwrite Config

12:10  Unipolar, INx referenced to COM

9:7      channel (Don't care at this point)

6        1/4 BW

5:3      External reference, internal buffer, temperature disabled

2:1      Disable Sequencer

0         read back current config

So the process to get where I'm at is as follows:

Startup system

Configure SPI Port (4MHz clock, 8 bit data, etc)

create Rising edge on CNV line

Lower CNV

Write config

Read back config

Perform 2 dummy conversion

Read config

Is there anything wrong with the process I'm taking?  Am I correct in thinking that the 14 bit configuration register is left justifed (MSB first) on both the transmit and receive?  I'm trying to use the device in RAC mode and I've attached a screen shot of the SPI Comms.

Any help would be greatly appreciated.

Regards,

Justin

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:44 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:44 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data