Post Go back to editing

AD7739 AIN Protection

The AD7739 datasheet states that the device can operate with +/- 2.5 volt inputs.

The Absolute Maximum ratings for the AIN pins are listed as -0.3V to AVDD + 0.3V which would appear to contradict the input voltage range.

I wish to use the device with an external instrumentation amplifier operating with supplies of ca +/- 15V and a ouput voltage range of +/- 2V in normal operation.

How should I protect the input of the AD7739 from overvoltage ouput of the instrumentation amplifier.

Parents
  • Hi Lyn,

    May I also suggest that you look at the AD7734 and AD7738 parts which may fit your needs.

    The AD7734 will accept bipolar signals using by it's internal biasing network. The AD7738 is similar in functionality to the previously mentioned part and also includes the MUX OUT pins allowing for only a single amplifier to work for all channels (providing it can settle fast enough).

    If you would like to provide some more information on your application we can help you with selecting some products to suit.

    Regards,

    Rob

Reply
  • Hi Lyn,

    May I also suggest that you look at the AD7734 and AD7738 parts which may fit your needs.

    The AD7734 will accept bipolar signals using by it's internal biasing network. The AD7738 is similar in functionality to the previously mentioned part and also includes the MUX OUT pins allowing for only a single amplifier to work for all channels (providing it can settle fast enough).

    If you would like to provide some more information on your application we can help you with selecting some products to suit.

    Regards,

    Rob

Children
No Data