Post Go back to editing

AD7763 Filter Download Question

Hi,

 

I am having problems downloading filters to the AD7763. I have tried the example in the datasheet (in Table 16) so that I know the checksum is correct but I am not getting the FILTER_OK or DL_OK bits set in the Status read (the other bits of the Status read are fine - and UFILTER is set).

 

I am convinced that I have no problems with the data timing and I have a good clean clock, frame sync and data. I am clocking at 12.8 MHz.

 

I would be grateful for answers to the following questions:

 

1. Are there are any errors or omissions in the datasheet with respect to the download?

2. Is there any difference between the effects of applying a hardware SYNC (via the SYNC pin) or writing to the SYNC bit in Control Register 1?

3. In Table 16 it is not clear whether the delay for the checksum should be before or after writing the checksum, could you clarify this please?

 

Many thanks,

 

Gary Moore

Parents
  • Hi Chris,

    My configuration is as follows:

    I have 4 AD7763s running together using MCLK = 25.6 MHz and with CDIV = 0 so that ICLK = MCLK/2 = 12.8 MHz.

    We have the decimation set to x16 so our output sample rate is 100 kHz.

    In an earlier version of our design we were running with CDIV = 1 and I’m fairly sure that this worked OK, i.e. we could successfully download the filter. Unfortunately it is not straightforward to re-create that arrangement.

    As I said in my response to Francois, it's possible that my problems are caused by the SYNC pulse width as we discovered that it wasn't as wide as we intended. I have not tried the download since we fixed that but I will let you know if this is successful.

    Thanks,

    Gary

Reply
  • Hi Chris,

    My configuration is as follows:

    I have 4 AD7763s running together using MCLK = 25.6 MHz and with CDIV = 0 so that ICLK = MCLK/2 = 12.8 MHz.

    We have the decimation set to x16 so our output sample rate is 100 kHz.

    In an earlier version of our design we were running with CDIV = 1 and I’m fairly sure that this worked OK, i.e. we could successfully download the filter. Unfortunately it is not straightforward to re-create that arrangement.

    As I said in my response to Francois, it's possible that my problems are caused by the SYNC pulse width as we discovered that it wasn't as wide as we intended. I have not tried the download since we fixed that but I will let you know if this is successful.

    Thanks,

    Gary

Children
No Data