Post Go back to editing

Driving AD7150 as a slave via I2C

Hi All,

I am trying to figure out how to control my AD7150 eval board using an external microcontroller (Cypress PSOC 4 Pioneer dev. kit). Does anyone have a step-by-step solution to do this, preferably with application code in the C programming language? More specifically, I'm trying to retrieve data from the AD sensor, convert it into a string, and pipe it through a serial port.

I've also recently obtained some AD7143 chips which I guess I will have to hand-solder onto a proto-board. At least on the software side, if not the physical configuration, is achieving the same goal with these chips as opposed to the AD7150 board pretty much the same? Or is it significantly different?

Thanks so much!

Parents
  • Hi Sean,

    Thanks for your response! Yes, I plan on connecting via J5. Additional question, though, how do I make that physical connection? From the external board, I'm running jumper wires, but on the AD7150, the pins are male rather than female. Do I just use alligator clips? That sounds like a weird way to make a digital connection. Also, must I, and how do I, tie the grounds of the two boards together?

Reply
  • Hi Sean,

    Thanks for your response! Yes, I plan on connecting via J5. Additional question, though, how do I make that physical connection? From the external board, I'm running jumper wires, but on the AD7150, the pins are male rather than female. Do I just use alligator clips? That sounds like a weird way to make a digital connection. Also, must I, and how do I, tie the grounds of the two boards together?

Children
No Data