Post Go back to editing

ADC used for single-pulse conversion

Hi guys,

I am looking for a low cost ADC for a single conversion on an external trigger (ECL logic). The trigger comes exactly at the peak amplitude of the pulse (pulse-width < 20ns). I have found the AD9070 which is unfortunately an obsolete product. The digital outputs should be TTL (not ECL) but the conversion-start trigger should be ECL, otherwise (if using an ECL to TTL converter) the maximum amplitude is not hit anymore.

Input voltage range: 0 to 2.5V or 5V

no of bits: 10 or more

the speed of the ADC is not really important as we do not need to detect all pulses (only for monitoring purposes).

any suggestion is welcome!

thx

PS: I have posted this question originally in the High-Speed ADC section, but it seems that they only have a pipelined structure which would not help me.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.