Ultra low power data collection - reading strain guage

I have a customer that needs to digitize the output of a strain gauge.  Their power source can vary from 1.6 to 3.6V and is capable of supplying no more than 200 uA.  Ideally, they want to use a differential input A/D and want a SPI output.  Sample rate is super low.  Maybe one sample per minute.  8 bit accuracy is acceptable.  The design is high volume 100-200K units and very cost sensitive  The Maxim MAX1391 is being considered.  As an alternative, I offered the AD7468 + AD8237.  I have a few questions:

  • Do we have a differential input, low cost A/D that can operate at 1.6V?
  • The 7468 datasheet recommend using the ADR318 as a reference/power supply for the ADR318 as a 1.8V reference.  This part is EOL.  I don't see another 1.8V reference to choose from.  Please offer suggestions of 1.6 or 1.8V references.  The customer does not want to use a higher voltage reference.
  • I assume that if the reference can source enough current, there would be no problem powering the AD8237 with it either.  Do you agree?
  • Can you propose any lower power or cheaper away to solve this problem?

Attached is my initial idea

A couple new thoughts.  Perhaps the AD8236 is a better fit for the Instrumentation amp.  It is much lower power.  Regarding the reference, I looked for something cheaper than the Maxim part and considered the following:

Both are very low power

Scan_Doc0008.pdf
Parents
  • 0
    •  Analog Employees 
    on Feb 6, 2014 11:21 PM

    Sorry to keep commenting.  Perhaps I should have thought about this more before posting.

    It occurs to me now that maybe I really don't need the reference.  As long as I power everything off the same power rail, the measurements should scale, right?  Also, if I have a 1.8V reference/ power supply for the A/D and IA, I won't be able to measure anything above 1.8V.  Right now, I'm feeling pretty silly.

    At this point, I'll just wait for your potential solutions.  Hopefully, I've describe the problem in an adequate fashion.

    Sorry

Reply
  • 0
    •  Analog Employees 
    on Feb 6, 2014 11:21 PM

    Sorry to keep commenting.  Perhaps I should have thought about this more before posting.

    It occurs to me now that maybe I really don't need the reference.  As long as I power everything off the same power rail, the measurements should scale, right?  Also, if I have a 1.8V reference/ power supply for the A/D and IA, I won't be able to measure anything above 1.8V.  Right now, I'm feeling pretty silly.

    At this point, I'll just wait for your potential solutions.  Hopefully, I've describe the problem in an adequate fashion.

    Sorry

Children
No Data