Post Go back to editing

Ultra low power data collection - reading strain guage

Thread Summary

The user seeks a differential input, low-cost A/D converter for digitizing strain gauge output, operating from 1.6V to 3.6V with a 200 uA power supply, 8-bit accuracy, and SPI output. The AD7687 is suggested as a differential ADC with an external reference, but it requires a 2.5V supply. The AD7793, AD7798/99, and AD7190 are recommended as single-chip sigma-delta ADCs with on-chip references, suitable for low-power strain gauge applications. The user also considers the AD8236 as a lower-power instrumentation amplifier.
AI Generated Content

I have a customer that needs to digitize the output of a strain gauge.  Their power source can vary from 1.6 to 3.6V and is capable of supplying no more than 200 uA.  Ideally, they want to use a differential input A/D and want a SPI output.  Sample rate is super low.  Maybe one sample per minute.  8 bit accuracy is acceptable.  The design is high volume 100-200K units and very cost sensitive  The Maxim MAX1391 is being considered.  As an alternative, I offered the AD7468 + AD8237.  I have a few questions:

  • Do we have a differential input, low cost A/D that can operate at 1.6V?
  • The 7468 datasheet recommend using the ADR318 as a reference/power supply for the ADR318 as a 1.8V reference.  This part is EOL.  I don't see another 1.8V reference to choose from.  Please offer suggestions of 1.6 or 1.8V references.  The customer does not want to use a higher voltage reference.
  • I assume that if the reference can source enough current, there would be no problem powering the AD8237 with it either.  Do you agree?
  • Can you propose any lower power or cheaper away to solve this problem?

Attached is my initial idea

A couple new thoughts.  Perhaps the AD8236 is a better fit for the Instrumentation amp.  It is much lower power.  Regarding the reference, I looked for something cheaper than the Maxim part and considered the following:

Both are very low power

Scan_Doc0008.pdf
  • Hi,

    We ar looking in to this. We'll get back t you soon.

    Regards,

    Jonathan

  • Thanks.  Hopefully my question makes sense.  The part I really hate is not having a reference solution.  I'd like to avoid recommending an Intersil or TI part if possible.

  • Hi Lionell,

    No worries on keeping commenting. It always help because, it can be give a better understanding of the problem.

    I found an ADC that is differential that is supplied from 2.5V to 5.5V. The AD7687 one of the candidates I found. The reference pin is external and can be connected with the power supply. The reference input voltage range from 0.5V to VDD+0.3. There is a circuit note for the AD7687 that you might want to check CN0225, http://www.analog.com/en/circuits-from-the-lab/CN0225/vc.html, Analog Front signal conditioner for industrial process control.

    From what I understand, the stimulus or analog voltage measured on  strain gauge are not dynamic. Usually for application that are not dynamic input voltage,sigma-delta ADCs are recommended.

    I would recommend, you may check Sigma Delta ADC I found which is a single chip solution for strain gauge application. To mention are the AD7793 ( has on chip reference), AD7798/99 and AD7190.

    Regards,

    Jonathan

  • Sorry to keep commenting.  Perhaps I should have thought about this more before posting.

    It occurs to me now that maybe I really don't need the reference.  As long as I power everything off the same power rail, the measurements should scale, right?  Also, if I have a 1.8V reference/ power supply for the A/D and IA, I won't be able to measure anything above 1.8V.  Right now, I'm feeling pretty silly.

    At this point, I'll just wait for your potential solutions.  Hopefully, I've describe the problem in an adequate fashion.

    Sorry

  • Thanks Jonathan.  I appreciate your input. The problem I have is that the solution must operate from a supply voltage of 1.8V to 3.6V.  A solution that requires a 2.5V A/D will not fit this application.

  • Hi Lionel,

    Do you know if the bridge will generate both positive and negative voltages? Or are they interested in the positive swing only? In any case, it may be necessary to shift the output to account for bridge offsets and/or negative voltages. I noticed this is missing from your sketch.

    Also, how much gain do they need and how large is the bridge offset? The following article may shed some light into why I'm asking

    http://www.analog.com/library/analogdialogue/archives/48-01/bridge_sensors.html

    Regards,

    Gustavo

  • Hello

    I'm pretty new in the forum I don't have much experience in fact this is my first cuestion in the forum, I was wondering if you could help me to find a sollution a similar problem that Lionelwallace has exposed time ago.

    I need to digitize the output of a strain gauge.  Their power source normally will be close to 3.6 but it should be possible use a step up for use with 5 v  the consumption is critically I mean must be very, very low consumption this circuit need the positive swing only, and the resollution must be  at least 10 bits  Ideally 12,  SPI output.  The maximum sample rate is 15ms.


    Could you please help me to find a sollution


    Thanks in advance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.