Post Go back to editing

AD7294-2

Hello,

Can I drive evaluation board AD7294-2 with Arduino Uno? I tried to establish connection on I2C bus without success.

Thank you in advance,

Svetlana

Parents
  • Hi,

    It looks like you are doing a read from  a write-only register (as per Table 9, address 0x00 is for the command register and it is write only). Can you do a read of another register with read or read/write access and see if you get an acknowledge bit?

    Also, can you double check if the evaluation board actually has pullup resistor? If you can, kindly send me a snapshot of your board.

    Regards,

    Karen

Reply
  • Hi,

    It looks like you are doing a read from  a write-only register (as per Table 9, address 0x00 is for the command register and it is write only). Can you do a read of another register with read or read/write access and see if you get an acknowledge bit?

    Also, can you double check if the evaluation board actually has pullup resistor? If you can, kindly send me a snapshot of your board.

    Regards,

    Karen

Children
No Data