AD7626 Ref input current value

Hi to all,

my acquisition and processing board has 12 AD7626 channels interfaced with a FPGA.

I have to provide a voltage reference source for all ADCs in simultaneous acquisition mode at 10MSPS.

So, following the application note "Voltage Reference Design for Precision Successive-Approximation ADCs" by Alan Walsh,

I choose the topology using a unit gain op-amp amplifier for each ADC (each op-amp fed from a unique ADR4540 voltage reference): see the topology below suggested in the AD7626 datasheet.

Supposing a AD7626 Vref input current value of 3.3mA average (10 times the AD7980; 1MSPS Pulsar ADC), I should

select a op-amp with internal output impedance low as 0.01 Ohm at 10MHz: this value is too low even for hi-speed op-amp like ADA4841.

So my question is regarding the AD7626 Ref input current value: is my hypothesis correct (Iref = 10 * Irref_AD7980)?

May be the AD7626 has a different internal topology and, for this reason, the Iref value is negligible and is not provided?

Thank you for any help.

reference_design.pdf
Parents
  • 0
    •  Analog Employees 
    on Nov 19, 2014 7:33 PM

    Hi Marco,

    The reference current draw of the AD7626 is not 10*AD7980. It's not specified in the datasheet but typically ~600uA. In the article you will see that i state the impedance at higher frequencies is handled by the 10uF cap. For example at 10MHz the impedance of the 10uF cap is 0.0016 ohms which is more than good enough to handle any noise/disturbance at the sample rate. The buffer really only needs to have low impedance from DC up to either the input signal bandwidth your interested in or where the impedance of the capacitor becomes low enough that the buffer output impedance no longer matters. Whats your input signal bandwidth? Also this is meant as a guideline, the output impedance calculated is for 0.5lsb droop in the reference, you may be able to handle more droop. It will just mean an extra gain error term in your conversion result. The AD8031 and ADA4841 should work fine as buffers here. There is also an even newer ref buffer the ADA4805-1 which has better offset and drift numbers.

    Best Rgds,

    Alan

Reply
  • 0
    •  Analog Employees 
    on Nov 19, 2014 7:33 PM

    Hi Marco,

    The reference current draw of the AD7626 is not 10*AD7980. It's not specified in the datasheet but typically ~600uA. In the article you will see that i state the impedance at higher frequencies is handled by the 10uF cap. For example at 10MHz the impedance of the 10uF cap is 0.0016 ohms which is more than good enough to handle any noise/disturbance at the sample rate. The buffer really only needs to have low impedance from DC up to either the input signal bandwidth your interested in or where the impedance of the capacitor becomes low enough that the buffer output impedance no longer matters. Whats your input signal bandwidth? Also this is meant as a guideline, the output impedance calculated is for 0.5lsb droop in the reference, you may be able to handle more droop. It will just mean an extra gain error term in your conversion result. The AD8031 and ADA4841 should work fine as buffers here. There is also an even newer ref buffer the ADA4805-1 which has better offset and drift numbers.

    Best Rgds,

    Alan

Children
No Data