Problem reading output from AD7961 FMC Board in Zedboard.

Hi,

I am using the EVAL_AD7961_FMCZ board to read values from the ADC into the Zedboard. I got the ADC verilog driver file from the Analog Devices WIKI project that uses AD7961 that has the following interface:

module AD7961

(

input m_clk_i, // 100 MHz Clock, used for tiing

input fast_clk_i, // Maximum 300 MHz Clock, used for serial transfer

input reset_n_i, // Reset signal, active low

input [ 3:0] en_i, // Enable pins input

input d_pos_i, // Data In, Positive Pair

input d_neg_i, // Data In, Negative Pair

input dco_pos_i, // Echoed Clock In, Positive Pair

input dco_neg_i, // Echoed Clock In, Negative Pair

output [ 3:0] en_o, // Enable pins output

output cnv_pos_o, // Convert Out, Positive Pair

output cnv_neg_o, // Convert Out, Negative Pair

output clk_pos_o, // Clock Out, Positive Pair

output clk_neg_o, // Clock Out, Negative Pair

output data_rd_rdy_o, // Signals that new data is available

output [15:0] data_o // Read Data

);


So making use of the AXI4Lite I have designed a hardware that reads and latches the value of data_o when the data_rd_rdy_o goes high. I debugged the hardware using ILA and the output wasn't as expected.

The first signal is the data_o (only last 16bits) and the second signal is the data_rd_rdy_o. The third one is where I latch the value of data_o. The data output looks strange as

  • Looks like data keeps accumulating till the data_rd_rdy_o goes high but it suddenly accumulates to zero sometimes.
  • The data output value is always zero or 21 (hex) no matter what input I give to the board.

Could some one please point out what could have gone wrong?


Heres my hardware setup :



Thanks.

Parents
  • 0
    •  Analog Employees 
    on Feb 8, 2015 9:34 PM

    Hi, Shan.

    Yes. You may set EN = 0001. Or you may still have it at 0010 but change LK7 to use the 4.096V REF from the ADR4540. The 2_048V REFIN is actually a test point for the ADR4520 output, thus the 2.048V you are seeing. I verified and REFIN is connected to GND with JP7 connected B to center.

    Regards,

    Karen

Reply
  • 0
    •  Analog Employees 
    on Feb 8, 2015 9:34 PM

    Hi, Shan.

    Yes. You may set EN = 0001. Or you may still have it at 0010 but change LK7 to use the 4.096V REF from the ADR4540. The 2_048V REFIN is actually a test point for the ADR4520 output, thus the 2.048V you are seeing. I verified and REFIN is connected to GND with JP7 connected B to center.

    Regards,

    Karen

Children
No Data