Post Go back to editing

AD7719 crystal oscillator specification?

Hi all,

In the datasheet AD7719 , there is not crystal oscillator specification @32.768 kHz typ.

How value is following specifications?

Crystal oscillator specification

Logic Inputs, XTAL1 Only

VINL, Input Low Voltage: ? V

VINH, Input High Voltage: ? V

Crystal Equivalent Series Resistance:min/typ/max ? kΩ

Crystal Frequency:min ? /32.768(typ)/ max ? kHz

XTAL1 Input Capacitance: ? pF

XTAL2 Output Capacitance: ? pF

Best Regards,

sss