appropriate ADC evaluation board

I am designing a single bit sigma delta ADC. My BW is 50mHz to 250Hz. Sampling frequency is 32kHz or 64kHz. To get a hands-on on testing the ADC, I am looking for an evaluation board with a similar ADC. Can u suggest me a suitable evaluation board for the same ? It would be good if I can view the output both at the 1-bit internal quantizer and the output of the decimation filter.

  • 0
    •  Analog Employees 
    on Mar 18, 2015 10:04 PM over 5 years ago

    Hi Jovialjha,

         Below is the short list of Sigma delta ADC that possibly fit to your requirement.

         ADI Sigma-Delta ADC portfolio range from 8bit to 24 bit resolution. And these parts are available with their evaluation board and software, you can visit ADI website Analog Devices | Mixed-signal and digital signal processing ICs  for details. In case you wanted search other products base from your specification, you use parametric search .Please refer to link Selection Table for Precision below.

    These ADCs are already packaged and access to the output quantizer might not be possible. There is the Dout, pin which outputs the conversion results.

    Part # Device Primary
      Function
    Resolution Throughput Rate # ADC Inputs FPBW (typ) Vsupply
      Positive (min)
    Vsupply
      Positive (max)
    Power
      Dissipation (typ)
    Operating Temp
      Range
    Package
    AD7787 Precision 24 120 SPS 2 28 Hz 2.5 5.25 800 µW -40 to +105 10 ld MSOP
    AD7791 Precision 24 120 SPS 1 28 Hz 2.5 5.25 800 µW -40 to +105 10 ld MSOP
    AD7790 Precision 16 120 SPS 1 28 Hz 2.5 5.25 800 µW -40 to +105 10 ld MSOP
    AD7709 Precision 16 105 SPS 4 25 Hz 2.7 5.25 8.8 mW -40 to +85 24 ld TSSOP
    AD7719 Precision 24 105 SPS 6 25 Hz 2.7 5.25 10 mW -40 to +85 28 ld TSSOP,28 ld
      SOIC - Wide
    AD7707 Precision 16 500 SPS 3 131 Hz 2.7 5.25 3.75 mW -40 to +85 20 ld SOIC - Wide,20
      ld TSSOP
    AD7706 Precision 16 500 SPS 3 131 Hz 2.7 5.25 6.5 mW -40 to +85 16 ld PDIP,16 ld
      TSSOP,16 ld SOIC - Wide
    AD7705 Precision 16 500 SPS 2 131 Hz 2.7 5.25 6.5 mW -40 to +85 16 ld PDIP,16 ld SOIC
      - Wide,16 ld TSSOP
    AD7730L Precision 24 600 SPS 2 23.4 Hz 4.75 5.25 32.5 mW -40 to +85 24 ld SOIC - Wide,24
      ld TSSOP
    AD7731 Precision 24 6.4 kSPS 3 31.6 Hz 2.7 5.25 67.5 mW -40 to +85 24 ld PDIP,24 ld SOIC
      - Wide,24 ld TSSOP
    AD7715 Precision 16 500 SPS 1 200 Hz 3 5.25 9.5 mW -40 to +85 16 ld PDIP,16 ld SOIC
      - Wide,16 ld TSSOP
    AD7713 Precision 24 205 SPS 3 53 Hz 4.75 10.5 5.5 mW -55 to +125 24 ld PDIP,24 ld SOIC
      - Wide

                                                                                               

             

    Regards,

    Jonathan                                                                             

  • 0
    •  Analog Employees 
    on Aug 2, 2018 2:56 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin